|
Configure the graph settings such as units/division, offset, and number of digits. |
|
Enable or disable vertical markers in the Single Chart view only. For more information, see Markers. |
|
Enable or disable horizontal markers in the Single Chart view only. For more information, see Markers. |
|
Area zoom. Use mouse to draw a frame around the desired area of the trace to zoom in on. |
|
Zoom in horizontally. To zoom in vertically only, click on the trace (trace turns into a thick line) and zoom in. Click the trace again to return to the normal zoom mode. |
|
Zoom out horizontally. To zoom out vertically only, click on the trace (trace turns into a thick line) and zoom out. Click the trace again to return to the normal zoom mode. |
|
Auto scale the trace on both the x- and y-axis. |
|
Auto scale the trace on the x-axis. |
|
Auto scale the trace on the y-axis. |
|
Automatically scroll new trace data from the right side of chart. Click the drop-down arrow next to this icon to auto scale the x-axis, y-axis, or both when appending new trace data. |
Right-click anywhere on the chart to display these options:
Save Chart Image to File - Export a screen shot of the chart to a JPEG, BMP, or PNG file, with a white grid on a black background. By default, the screen shot is stored in the "My Documents" folder on your computer. For example – C:\Users\<user_name>\Documents\Keysight\BenchVue\Oscilloscope\Exports\.
Copy Chart Image to Clipboard - Export a screen shot of the chart to the Windows clipboard.
Vertical Marker 1|2 - In the Single Chart view only, you can enable and disable vertical markers from the right-click menu.
Horizontal Marker 1|2 - In the Single Chart view only, you can enable and disable horizontal markers from the right-click menu.